Measure and evaluate heating currents and use them for process reliability
The heating current measurement is an important addition to the functional scope of the controller.
Every Meusburger controller or control system is prepared for heating current measurement. There are 2 measurement methods (individual current measurement and total current measurement) that can be used depending on the series. Several current transformer types are available for the heating currents to be measured.
Each control zone has its own measurement input and is measured with its own current transformer. Depending on the heater used (single-phase heater, three-phase heater), up to three single-phase current transformers or one three-phase current transformer can be used per zone.
Multiple heating zones are measured with one current transformer and only require one measurement input on the controller. Therefore, an assignment of control zone and current transformer must be planned. Depending on the heaters used (single-phase heaters, three-phase heaters) and the phase distribution of the heaters, up to three single-phase current transformers or one three-phase current transformer can be used for each measuring input.the heating currents for each control zone are measured one after the other. The measuring process is controlled by the controller. The controller ensures that the heating current of each control zone is measured separately.
| Reglerbaureihe | Anzahl Messeingänge / Anzahl Phasen | Einzelstrom-messung | Summenstrom-messung | Hinweis |
|---|---|---|---|---|
| ETR 46 | 1 x einphasig | x | ||
| sysTEMP ETR 132 | Pro Modul 8 x dreiphasig | x | x | |
| sysTEMP ETR 112 | 2 x dreiphasig | x | Über CANSTI | |
| sysTEMP ETS 132 | 2 x dreiphasig | x | ||
| flexoTEMP DIO 16 CI | 1 x dreiphasig | x | Für die auf dem Modul projektierten Zonen | |
| flexoTEMP DIO 32 CI | 2 x dreiphasig | x | Für die auf dem Modul projektierten Zonen | |
| THYPO TP | x | Im Modul integriert, Messung rückwirkungsfrei auf Regelung. |
Mains voltage measurement modules can be used to reduce the influence of mains voltage fluctuations on the measured heating current. The heating current displayed is corrected by calculation using the measured mains voltage.